OSBDM Bugs - Who to send fixes to?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSBDM Bugs - Who to send fixes to?

3,393 Views
pgo
Senior Contributor V
Dear All,

I've found what I believe are some bugs in the OSBDM code.  To whom should fixes be directed?

Summary:

The following Low level BDM routines are incorrect (They all expect ACKN which does not occur for these commands,  This ends up disabling the ACKN operation):

BDM08_CMD_READSTATUS
BDM08_CMD_WRITECONTROL
BDM08_CMD_READ_BKPT
BDM08_CMD_WRITE_BKPT

bye
Tags (2)
0 Kudos
Reply
2 Replies

801 Views
osbdm_support
Contributor II
Hi pgo,

You can send your fixes to me for review.

Thanks!

Dan

0 Kudos
Reply

801 Views
pgo
Senior Contributor V

Dear Dan,

Attached is a text file that lists what I believe are some minor bugs in the OSBDM code.

The example code is from the USBDM code posted elsewhere so does not correspond exactly with the changes needed in OSBDM but should be sufficient to indicate what to look at.

Please let me know if anything is unclear or if I am mistaken.

Bye

 

Fixes1.txt

Message Edited by t.dowe on 2009-10-26 05:07 PM
0 Kudos
Reply