My problem with S12X and the TBDML

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

My problem with S12X and the TBDML

5,888 次查看
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Fri Sep 09, 2005 1:06 am    
 
Dear all:
Now we want to use S12X controller. And we have used HCS12 controller before. And we have the TBDML simulator, but now we wonder that if the TBDML can be used in the S12X controller? Thanks and we are eager for your answer.
 
Posted: Fri Sep 09, 2005 7:06 am    
 
TBDML has no problem talking to S12X, I am using it with XDP512 almost every day without any problems.
Posted: Mon Oct 31, 2005 4:42 am    
 
The tbdml might work with the S12X, but it doesn't implement all of the available functionality that a S12X BDM could, like setting break points for XGATE, etc.

To get a feeling for what can be done via BDM, see section 18 and 19 of the 9S12XDP256 users guide, which cover the BDM and Debugging modules.
 
Posted: Thu Nov 03, 2005 12:33 pm    
 
Setting breakpoints is not a job for the cable. That is a job for the debugger. Do not mix the two tools together please.

The metrowerks S12X capable debugger works with TBDML.
0 项奖励
回复
2 回复数

802 次查看
naclchan
Contributor I

Hi:

 

   I am a starter on BDM,I want to know if my MC9S12XF512 can talk to TBDML 

0 项奖励
回复

802 次查看
UcTechnoGeek
Contributor II

First check if Codewarrior supports development with the TBDML for that particular device.

 

- Is the TBDML available as a target when you create the project for that micro?

 

Second - The TBDML (assuming you have the JB16 version) will be limited to a max bus frequency of 20Mhz (usually 1/2 the crytal speed).

0 项奖励
回复