Multiple OSBDM connections and CW10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple OSBDM connections and CW10

751 Views
admin
Specialist II

I want to connect a couple boards via OSBDM. As far as I can judge, OSBDM is able to support multiple connected devices. But it looks like CW10 always connects to device #0, that is the first detected device, I guess.

 

What can I do with CW10 settings to make it debug another device (#1)? Is there any GDI connection attribute that may help here? I do not want to reverse-engineer the GDI dll really.

 

Thanks in advance

Tags (2)
0 Kudos
Reply
0 Replies