Hi, I am porting CW10 project to KDS and encounter difficulties when debugging with latest USBDM (V4.12.1.30). Our target is MK10DX128M7. I just created the simplest example project with main.c having for (;;) { i++; }. Compile and debug. It works fine. Then, in the linker file MK10DX128xxx7_flash.ld, just change from
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0001FBF0
to
m_text (RX) : ORIGIN = 0x10000000, LENGTH = 0x00008000
Recompile and debug. KDS IDE complains:
I am assuming the problem is that KDS IDE doesn't recognize the FlexNVM region. I search web and understand that since USBDM 4.9.5, it added support for FlexNVM partitioning in Kinetis devices. But in KDS IDE or USBDM, I can't find anywhere that allow me to set the region as legal.
Does anyone know a fix for this??
已解决! 转到解答。
Hi Jei,
I had not anticipated the debugger needing to program the FlexNVM so the GDB server is failing to report that range of memory as programmable.
I will correct this in the next release.
In the interim you can try the updated device file attached. This is a hack but it worked for a similar device.
You will need to replace the file "C:\Program Files (x86)\pgo\USBDM ....\DeviceData\arm_devices.xml" with the attached file.
Please advise if it works.