How do I re-flash a USBDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I re-flash a USBDM

ソリューションへジャンプ
1,672件の閲覧回数
juliancox
Contributor V

I have a "dead" JS16CWJ based USBDM. When I plug it in there is no activity on the COM LED and I believe that there is either a hardware fault or the Flash is corrupt. EXACTLY how do I re-flash it? I have another USBDM (JM60). Obviously I cannot use the USBDM app because, according to my computer, the board does not exist. How do I connect the two USBDMs together? I enclose a picture of the faulty board.pastedImage_1.jpg

0 件の賞賛
返信
1 解決策
1,490件の閲覧回数
juliancox
Contributor V

Since posting this I have been able to re-flash the board and it works with USBDM 4.12, but not with C/W as is the case with my other BDM How do I get tit to work with C/W?

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,491件の閲覧回数
juliancox
Contributor V

Since posting this I have been able to re-flash the board and it works with USBDM 4.12, but not with C/W as is the case with my other BDM How do I get tit to work with C/W?

0 件の賞賛
返信