Help Building PC executables (dll and test programs)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Help Building PC executables (dll and test programs)

跳至解决方案
2,784 次查看
osorakunakamori
Contributor I

First, let me offer huge praises to pgo and all other contributers who have done this fantastic work. Thanks so very much!

 

I want to build the PC-side programs of USBDM, namely the dll and test program. What do I need for this? I am guessing Eclipse and cygwin ... is this correct? Has anybody built them with VC++? Any advice to help a stranded newbie is much appreciated!!

 

Thanks! 

  

标记 (2)
0 项奖励
回复
1 解答
822 次查看
pgo
Senior Contributor V

Dear osoraku,

 

The DLL for USBDM were built with eclipse & MINGW.   It should be possible to to build them with VC++ but there are some environment variables that should be set for the different targets.  This is done as part of the eclipse setup and would be automatically done if the eclipse packages were imported into Eclipse.

 

bye

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
823 次查看
pgo
Senior Contributor V

Dear osoraku,

 

The DLL for USBDM were built with eclipse & MINGW.   It should be possible to to build them with VC++ but there are some environment variables that should be set for the different targets.  This is done as part of the eclipse setup and would be automatically done if the eclipse packages were imported into Eclipse.

 

bye

 

0 项奖励
回复