HI-WAVE Warning: "DBG module is armed. Disarm?"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HI-WAVE Warning: "DBG module is armed. Disarm?"

ソリューションへジャンプ
1,333件の閲覧回数
carloscuev
Contributor V

Im working with a Witztronics hardware with updated USBDM v4.4-Beta Firmware. Im programming a S08JM60, Every breakpoint or debug command (except Start, Single Step and Step Over), hiwave keeps asking me  "DBG module is armed. Disarm?" and clicking "Yes" or "No" it works fine, I can debug without any problem, but the popup window is quite annoying, Is there something cand be done about this?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
785件の閲覧回数
carloscuev
Contributor V

Solution Found:

In Debugger Check Option "HCS08 Open Source BDM->Trigger Module Settings->General Settings->Disarm automatically the module when debugger stops"

 

Now I like more USBDM than USB-MULTILINK-BDM :smileyvery-happy:

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
786件の閲覧回数
carloscuev
Contributor V

Solution Found:

In Debugger Check Option "HCS08 Open Source BDM->Trigger Module Settings->General Settings->Disarm automatically the module when debugger stops"

 

Now I like more USBDM than USB-MULTILINK-BDM :smileyvery-happy:

0 件の賞賛
返信