Hi all, and particularly PGO,
I'm experimenting issues with CodeWarrior10.6 and the USBDM with DSC MC56F8345 or MC56F84789 device. I have created a project and keep all default options. However, it is not possible to load and debug the application. I get the following error when launching the debugging:

In the console:
Executing Initialization File: E:\Codewarrior\84789_BDM/Project_Settings/Debugger/MC56F84789.tcl
radix x
cmdwin::eclipse::config hexprefix 0x
cmdwin::eclipse::config MemWidth 16
cmdwin::eclipse::config MemAccess 16
cmdwin::eclipse::config MemSwap off
Starting 3rd party flash programming...
DiMemoryDownload() - DI_DNLD_TERMINATE - Programming memory image...
===========================================================
Programming target
Device = 'MC56F84585'
Trim, F=0, NVA@0000, clock@0000
Ram[0000...3FFF]
Erase=EraseMass
Security=intelligent
Total bytes=35556
doRamWrites=T
Erase Time = 3.48 s, Speed = 9.97 kBytes/s, rc = 0
DiMemoryDownload() - DI_DNLD_TERMINATE - Programming complete, rc = 7
Thanks for your attention,
Best Regards,
yongsheng