Dear pgo,
Thanks for the reply
I had enabled the BDM interface on the board and have confirmed it , because if i remove the BDM enable jumper
i get the error messsage very early and i cannot even see the dowloading progress bar.
Then i installed the DEBUG VERSION of USBDM( by double click on Install Codewarrior Debug Files.cmd),
In the command window i could see the installation messages
3 files copied for for code warrior for ColdFire V2,V3 &V4,
1 file copied for code warrior for RS08/HCS08/Coldfire v1,
1 file copied for code warrior for HCS12
Then i tried downloading the code into the RAM and i got the same error message:
"ColdFire GDI Protocol Adapter: An invalid preference was passed to the ColdFire GDI protocol "
Then i typed %APPDATA%\usbdm in the address bar of a Windows Explorer, but windows couldn't find that folder.
Even i went to application data folder and checked, but there was no usbdm folder.
Then i gave search in windows for *.log and i could locate one file in C:\ by name usbdm_dll.log
i am attaching this file, please check whether this is correct file and any error can be located in the log file.
bye