Hi!
If I'm correct, demo boards, like DEMOJM, DEMOAC and DEMOQE has and OSBDM wihtin them. I'm currently using both DEMOJM and DEMOAC to download code to my custom hardware.
I'm also working with TWRK60N512 and MQX. And printf is set (by default) to the OS-JTAG COM port.
My question is... can I do the same with DEMOJM and DEMOAC boards? I mean, are they also listed as COM ports? should I update OSBDM drivers?
What I'd like to do is use this printf for debugging, like a trace. (I'm not using MQX and no other RTOS on my custom hardware/firmware)
Thanks in advance!!
SebaS
Solved! Go to Solution.
Dear Sebasira,
I've only looked at the DEMOJM. It does not have an OSBDM. It has a Embedded Multilink. The manual (link below) refers to the ability to use a serial port over the USB, so it should be possible.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMOJM
I would expect it to use the P&E drivers. You could check their web site for the latest drivers.
bye
Dear Sebasira,
I've only looked at the DEMOJM. It does not have an OSBDM. It has a Embedded Multilink. The manual (link below) refers to the ability to use a serial port over the USB, so it should be possible.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMOJM
I would expect it to use the P&E drivers. You could check their web site for the latest drivers.
bye
Thank you pgo...
Here's a link to the P&E manual of the DEMOJM Board: http://www.freescale.com/files/microcontrollers/doc/user_guide/DEMOJMUM.pdf