Can't connect. The Debugger can not connect to the P&E device(HC/RS/S12Z GDI Protocol Adapter)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't connect. The Debugger can not connect to the P&E device(HC/RS/S12Z GDI Protocol Adapter)

343 Views
andy_Musk
Contributor III

Can't connect. The Debugger can not connect to the P&E device(HC/RS/S12Z GDI Protocol Adapter)

0 Kudos
Reply
2 Replies

213 Views
pgo
Senior Contributor V

Hi Andy,

Can you identify the programmer you are using a bit more clearly?

OSBDM programmer supported by P&E is only used in some development boards (e.g. https://www.pemicro.com/osbdm/osbdm_description.cfm)  There is an earlier version that is not supported - I don't know why they used the same name!

Also many of the OSBDM interfaces currently available are actually USBDM.

A picture may clarify the situation.

bye

0 Kudos
Reply

342 Views
andy_Musk
Contributor III

i am use CW11.1 and OSBDM programmer to program a  board base on MC9S08JM60CLD chip.  but i cannot success it,why?

0 Kudos
Reply