Can Usbdm read data from S9s12G64 mcu?
If, how to connect pin config and which application software should I use?
I bought usbdm last month.
But there is no Cd for to install u
sbdm software.
Help me please.
Hello Saw Eddie,
Yes, USBDM support this chip.
You need install USBDM software and driver , refer to this thread :
And if you use IDE, for example CWv5.2, please choose it when install USBDM software.
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear,
I bougt usbdm,js16-0001 and installed usbdm software and its driver.I
connected usbdm gnd to target mcu,s9212g64,gnd;
usbdm bkgd to mcu bkgd pin;
usbdm reset pin to mcu reset pin.
Then I powered mcu with other power source and detected it.It's ok.But when
I click read memory pop up menu show that connection with the target has
failed.
The question I want to know is how to connect usbdm and target mcu
successfully.
Thanks
Eddie.
Hello Eddie,
The USBDM is Open Source, and I know little about "js16-0001" ,
please find information or ask on this thread: https://community.nxp.com/community/bdm
it focus on the USBDM related question .
Hope it helps
Alice
Dear,
I only need to know how to connect usbdm and target mcu wiring
connection.Please send me if you have the connection diagram of usbdm and
target mcu,s9s12G64.
Thanks.
Eddie