Can Usbdm read data from S9s12G64 mcu?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Usbdm read data from S9s12G64 mcu?

3,048 Views
saweddie
Contributor II

Can Usbdm read data from S9s12G64 mcu?

If, how to connect pin config and which application software should I use?

I bought usbdm last month.

But there is no Cd for to install u

sbdm software.

Help me please.

0 Kudos
Reply
4 Replies

2,829 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Saw Eddie,

Yes, USBDM support this chip.

You need install USBDM software and driver , refer to this thread :

USBDM: Software Installation 

pastedImage_2.png

And if you use IDE, for example CWv5.2, please choose it when install USBDM software.

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,828 Views
saweddie
Contributor II

Dear,

I bougt usbdm,js16-0001 and installed usbdm software and its driver.I

connected usbdm gnd to target mcu,s9212g64,gnd;

usbdm bkgd to mcu bkgd pin;

usbdm reset pin to mcu reset pin.

Then I powered mcu with other power source and detected it.It's ok.But when

I click read memory pop up menu show that connection with the target has

failed.

The question I want to know is how to connect usbdm and target mcu

successfully.

Thanks

Eddie.

0 Kudos
Reply

2,828 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eddie,

The USBDM is Open Source, and I know little about "js16-0001" ,

please find information or ask on this thread: https://community.nxp.com/community/bdm 

it focus on the USBDM related question .

Hope it helps

Alice

0 Kudos
Reply

2,828 Views
saweddie
Contributor II

Dear,

I only need to know how to connect usbdm and target mcu wiring

connection.Please send me if you have the connection diagram of usbdm and

target mcu,s9s12G64.

Thanks.

Eddie

0 Kudos
Reply