Hello pgo,
I am posting a new question here as per your suggestion.
I am trying to connect my S12GA48 board with CW5.2 on Win10. I am using latest USBDM drivers from sourceforge site.
I am using USBDM based on JM60xx design. I can program my S12GA48 on my older Win7 board. I am following to patch CW5.2 missing variants as given below thread,
I can detect the S12GA48 with HCS programmer app in USBDM. So, no issues of USBDM detection and programming issue.
But, when I am trying to create the project in CW5.2, I am not able see the USBDM in connection window as shown in attached image.
Your help is appreciated. We have already purchased 100 S12GA48 CPUs.
Gavali N. K.
解決済! 解決策の投稿を見る。
Hi,
I'm not familiar with the process you have linked to.
The following may be useful but given the above I am unsure.
The USBDM installer modifies the files within the C:\Program Files (x86)\Freescale\CWS12v5.2\bin\Plugins\Support\HC12Wizard\XML to add the USBDM target. If the original XML file is not present when installing the software it will not be modified.
So .. You can check the following:
I will have a play with this in a while.
I note that the S12GA48 was added to CWS12v5.1 by a fix-pack.
https://www.nxp.com/docs/en/supporting-information/CW12_5-1_INST-INSTR-S12G-RMF.pdf
Can you use this version?
PS. There is no device entry for MC9S12GA48 in the USBDM software. Are you using MCS12GA240 to test the stand-alone programmer?
bye
Hi,
I'm not familiar with the process you have linked to.
The following may be useful but given the above I am unsure.
The USBDM installer modifies the files within the C:\Program Files (x86)\Freescale\CWS12v5.2\bin\Plugins\Support\HC12Wizard\XML to add the USBDM target. If the original XML file is not present when installing the software it will not be modified.
So .. You can check the following:
I will have a play with this in a while.
I note that the S12GA48 was added to CWS12v5.1 by a fix-pack.
https://www.nxp.com/docs/en/supporting-information/CW12_5-1_INST-INSTR-S12G-RMF.pdf
Can you use this version?
PS. There is no device entry for MC9S12GA48 in the USBDM software. Are you using MCS12GA240 to test the stand-alone programmer?
bye
Hello pgo,
The suggested xml file was already present in the directory.
I just uninstalled the USBDM and re-installed it.
Now it is working Win10 as well.
Thanks for quick suggestion. Great.
N. K. Gavali
Hello pgo,
I am now facing weird problem.
When I am trying to connect USBDM through CW5.2 IDE, then the debugger is not detected. Even if I tried to detect USBDM by pressing "DETECT" button. The problem is shown as the attached fig.
I can see that there is communication happening with debugger through IDE. The LED on USBDM (JM60xx board) not blinking.
if I have run the HIWAVE.exe utility separately, then USDBM can be detected correctly and I can connect to target.
Also, the USBDM can be detected in HCS12 programmer app and I can program the target.
The most surprising thing is, this problem is not facing on my home laptop with Win10. But, the problem can be seen in office laptop. The driver and USBDM version are same at both laptops.
I need to run the programming on office laptop for the code development.
Appreciated for help.
Thanks and Regards,
N. K. Gavali
Hi,
I'm equally surprised by your results, especially that you get different results when you run HIWAVE.exe stand-alone. I cannot think why you would get different results when HIWAVE.exe is launched from the main application.
Can you do the following to produce log files:
In the directory C:\Program Files (x86)\Freescale\CWS12v5.2\Prog\gdi
Arbitrary things to try:
For you own information the first few lines of the usbdm.log file will show the devices detected.
I have done some testing with a JS16 BDM - I will have to find a JM60 version for further tests.
bye
Hello pgo,
Thanks for the quick reply.
>>>>Can you do the following to produce log files:
>>>>>In the directory C:\Program Files (x86)\Freescale\CWS12v5.2\Prog\gdi
The USBDM and TBDML log files with standalone HIWAVE and with CW52 debugging are attached here.
I have deleted TBDML_Config.cfg file from the location. But no change.
Both folders are not identical. i386-win-gnu folder has more files than gdi folder.
Already tested with USB hub and still the same problem.
Serial# = USBDM-JMxx-0001
Hardware Version = USBDM - (JMxxCLD)
Software Version = 4.12
Flash Start = 0xC000
Protect Address = 0xFC00
Code Start Address = 0xC000
Code End Address = 0xFFFF
UserDetectICP() = 0xEE07
Thanks
N. K. Gavali
HI,
Thanks for the logs.
Sorry, I did not mean to imply that all the files would be present in GDI - merely that the ones there should be identical to the ones in the USBDM installation location i386-win-gnu.
The log doesn't really tell me much.
The process is failing very early on when the DLL tries to initialise libusb:
/* 0.07 */ USBDM_ErrorCode bdm_usb_init(): libusb_init() Failed, rc=-12, LIBUSB_ERROR_NOT_SUPPORTED
This doesn't occur for the stand-alone run.
libusb_init() doesn't even require the USBDM driver to be installed.
There are a few things about your logs that puzzle me but I have no idea what it means.
Things to try/check:
I will think about this a bit more but since I can't reproduce the problem its a bit hard to investigate.
bye
Ok. followed your suggestion.
Running IDE.exe in administrator mode solve the issue.
Bravo!!!!....Thank pgo for fantastic help.
Happy Weekend.
N. K. Gavali