NavQ boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NavQ boot

6,577 次查看
ahsunq
Contributor I

NavQ is not being detected by uuu on windows or mac, when NavQ is set to boot from USB. Trying to flash it just says "waiting for known USB device to appear.."

When NavQ is setup to boot from SD card, it seems to go through a boot from mmc1 and seems to be in a loop. Here is the snippet of the log from this mode. 

switch to partitions #0, OK
 is current device
28447232 bytes read in 1220 ms (22.2 MiB/s)
Booting from mmc ...
39567 bytes read in 17 ms (2.2 MiB/s)
## Flattened Device Tree blob at 43000000
   Booting using the fdt blob at 0x43000000
   Using Device Tree in place at 0000000043000000, end 000000004300ca8e
Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
failed to get any video link display timings
probe video device failed, ret -22

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.4.24-2.1.0+gbabac008e5cf (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Fri Jul 24 23:17:18 UTC 2020
[    0.000000] Machine model: NXP i.MX 8M Mini NavQ Board with LPDDR4 memory
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.

 

Any tips on getting NavQ up and running? 

0 项奖励
回复
3 回复数

6,538 次查看
ahsunq
Contributor I

The issue has been resolved - seems to have been due to power supply.

When using a fast USB-C charger to supply power, the device seems to be stuck in a boot cycle, although I re-call reading in the guide somewhere that a fast charger should work..

When power to the NavQ was supplied from the laptop, I was able to boot up fine and get to the Linux shell. 

0 项奖励
回复

6,544 次查看
Landon_Haugh
NXP Employee
NXP Employee

Can you send some pictures of your boot switches and screen when you're getting these errors?

Also, are you connected using the USB-C cable? You can not flash the board using the microUSB port.

0 项奖励
回复

6,550 次查看
iaingalloway
NXP Employee
NXP Employee

Thanks for your post - Let me get someone to reply on this.
Q: please confirm - did your NavQ boot from the factory? They were all tested before they were sent out.
I assume by your question you have already followed our guides here?
https://nxp.gitbook.io/8mmnavq/getting-started/quickstart/flash-sd-card-with-linux-image#flashing-th...

 

0 项奖励
回复