Wireless and Connected Home of the Future

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wireless and Connected Home of the Future

Wireless and Connected Home of the Future

Internet of Things nodes are using a wide plethora of heterogeneous wireless connectivity protocols such as: IEEE® 802.15.4, Thread, ZigBee®, 6LoWPAN/IPv6, and BLE. By attending this session you will learn which wireless communication protocol is the right solution for their application requirements, while comparing various communication protocols for 2.4 GHz and sub-1 GHz technologies. This session will provide an overview on commonly used wireless technologies and standards for smart homes and which Freescale microcontroller families are best suited for connected appliance, sensor device or hub product idea.

Presented by Antonio Concio

Presented at DwF Istanbul/Ankara - May 12/14, 2015

Session ID: EUF-IND-T1462

添付
評価なし
バージョン履歴
最終更新日:
‎05-04-2015 12:49 AM
更新者: