NXP Tech Blog - 9ページ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tech Blog - 9ページ

Kathleen
NXP Employee
NXP Employee

Continuing with my countdown of top reasons to use i.MX RT1010 crossover MCU, today I want to talk about performance.  The performance of the i.MX RT series really pushes this portfolio to a classification of its own – crossover MCUs. Engineers can now enjoy the level of performance historically seen in the processor space, now in the MCU world – providing tremendous familiarity and usability for engineers. But just ask the rabbit from the Tortoise and the Hare fable, sometimes it is not enough just to be fast. You have to be smart too. Within the i.MX RT1010 family, several smart features are coupled together with the 500 MHz Arm® Cortex®-M7 core.

詳細を読む...

件数が多いもの
0 0 2,439
vishakhadakhane
Contributor III

Hello everyone, I am working on MCUxpresso and using LPC1769 controller. I am done with Led blinking in MCUxpresso. I have used flash magic to flash the hex file in controller using usb to ttl. But I faced a hex file issue while doing this project. So I thought I should share this with everyone who are facing the same issue. After compiling only .axf was getting created. For creating .hex file ,you need to do following settings

詳細を読む...

件数が多いもの
1 1 10.9K
Kathleen
NXP Employee
NXP Employee

Continuing with my 10-day countdown to top reasons to consider the i.MX RT1010, today we look at reason #9 -the unlimited memory capabilities of the i.MX RT1010.

Looking at the i.MX RT1010 crossover MCU, one might notice that there is no on-chip Flash memory. Where do you boot from? Where do you store your code? And is it safe? What about latency issues? The i.MX RT1010 MCU was designed to ensure maximum memory flexibility, while not sacrificing performance or security.

詳細を読む...

件数が多いもの
0 0 2,052
Kathleen
NXP Employee
NXP Employee

As explained in my blog yesterday, for the next 10 days, I will countdown 10 top reasons to consider the i.MX RT1010 for your next design.  Today we start with reason #10 -the EVK.  Since the first i.MX RT crossover MCU first launched in 2017, the EVK has been the board of choice for developers. Right-sized with the right level of features and capabilities

詳細を読む...

件数が多いもの
0 0 2,022
iWave
Contributor V

iWave Systems, a leading embedded solutions provider company based in Bangalore has successfully demonstrated Xen virtualization hypervisor on their i.MX8 QM SoC based System on Module. The  multi-core SOM comprises of 2x Arm® Cortex® -A72 @1.8 GHz and 4x Arm® Cortex®-A53 @1.2 GHz and 2x additional Cortex®-M4F @ 266 MHz, rendering a highly powerful  integrated solution on a SMARC R2.0 compatible module.

詳細を読む...

件数が多いもの
0 0 4,458
Kathleen
NXP Employee
NXP Employee

Though not widely publicized, the $1 price point of the newly announced i.MX RT1010 crossover MCU made me pause. My parents always told me that a dollar is not what it used to be, meaning that the value of a dollar today does not go nearly as far as it used to for them when they were growing up.

詳細を読む...

件数が多いもの
1 0 2,386
omar_cruz
NXP Employee
NXP Employee

Searching for a low-power, well-integrated but cost-sensitive MCU for your embedded designs? Look no further – the K32 L2 MCU family is for you!

詳細を読む...

件数が多いもの
1 0 33K
martinformanek-
NXP Employee
NXP Employee

Dear MCUXpresso user,

 

We have decided to remove “Configurations” page from MCUXpresso SDK Builder website (http://mcuxpresso.nxp.com) with the December update this year.

Details are summarized below about the existing Configurations page and how page’s functionality will replaced.

詳細を読む...

件数が多いもの
1 0 3,710
lpcxpresso_supp
NXP Employee
NXP Employee

An issue has been identified that impacts the debugging of older LPC devices using SEGGER Jlink via the version of MCUXpresso IDE v11.0.1 released on 4th September 2019.

This issue will be seen only when debugging an LPC device that use the IDE's Preinstalled part support i.e. parts that do not require an SDK - a debug operation via SEGGER Jlink will lead to an error as below:

詳細を読む...

件数が多いもの
2 0 13.1K
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v11.0.1 (build 2563) is now available.

This is a maintenance release that builds upon the previous MCUXpresso IDE v11.0.0 release, and we recommend that all existing users download and install this new version. It also incorporates a minor update to the integrated MCUXpresso Config Tools.

詳細を読む...

件数が多いもの
0 0 5,240
KATE_WANG
NXP Employee
NXP Employee

Dear sdk developers,

During our development, more and more components are joining our sdk. It is necessary for the component sections recorded in yml data to follow a simple and effective naming convention, so that they can be well organized, identified and processed.

Here we provide the doc of Yml Data Record Component Naming Conventions, please kindly review and follow the rules in your future development.

詳細を読む...

件数が多いもの
0 0 1,756
raluca_popa
NXP Employee
NXP Employee

This tutorial demonstrates how to convert a Tensorflow model to TensorFlow Lite using post training quantization and run the inference on an i.MX8 board using the eIQ™ ML Software Development Environment. It uses a TensorFlow mobilenet_v1 model pre-trained with ImageNet.

NOTES:

1. Except for the section "Build Custom Application to Run the Inference" this tutorial can also be applied to any i.MX RT platform.

2. For more information on quantization check the 'QuantizationOverview.pdf' attached to this post.

詳細を読む...

件数が多いもの
6 0 8,416
lpcxpresso_supp
NXP Employee
NXP Employee

The Windows installer for SEGGER J-Link has changed behaviour for version after V6.44 i.e. after the version installed with V11.0.0 of the IDE. Previously each SEGGER installation was located in a versioned directory e.g. JLink_V644g, now each new installation will by default, write to C:\Program Files (x86)\SEGGER\JLink.

This change will only impact Windows users who manually install a later version of SEGGER J-Link for use within MCUXpresso IDE.

詳細を読む...

件数が多いもの
2 0 6,088
kuruibonny
Contributor III

I think this might be late since I was using Ubuntu 18.04 until recently when I upgraded to latest version 19.04

Tried to install Mcuxpresso IDE I encountered some dependency errors but managed to solved it. I had already replied to question about it but decided #to write main post about it.

詳細を読む...

件数が多いもの
0 0 5,464
CJarvis
NXP Employee
NXP Employee

In March of 2017, NXP released the debut version of the MCUXpresso SDK along with an IDE and set of Config Tools under the same MCUXpresso name.  Since that time we have seen an amazing response from developers downloading and using this suite of software and tools.  The number of MCUXpresso SDK downloads recently surpassed 100,000 unique downloads.

As the NXP and former Freescale microcontrollers were unified under one company, we knew we needed to provide a consistent and efficient software development platform – one that would allow you  the flexibility to develop on a wide range on NXP microcontrollers without the need to relearn a new software architecture or re-invent basic enablement functionality.

詳細を読む...

件数が多いもの
0 0 2,476
Ragan_Dunham
NXP Employee
NXP Employee

Machine Learning at the Edge:

eIQ Software for i.MX Applications Processors

Developing machine learning (ML) applications for embedded devices can be a daunting task. For the traditional embedded developer, the learning curve can be quite steep, as there are numerous decisions that must be made and new jargon that must be learned. Which framework should I choose? Which model best meets the requirements of my application and how do I know when it’s good enough? What “size” microcontroller or application processor do I need? The questions are many and figuring out how to get started can prove to be a challenge.

詳細を読む...

件数が多いもの
2 7 22K
brendonslade
NXP TechSupport
NXP TechSupport

LPC845 Breakout Board now has an SDK package available! We are working on updating our getting started information to show how to use this rather than starting from the LPC845 chip SDK. The board is called LPC845BREAKOUT in the SDK builder.

詳細を読む...

件数が多いもの
1 0 1,570
nxf39066
NXP Employee
NXP Employee

If you need to create you own SuperSet, following steps should help you.

First of all you need mcu-sdk-2.0 repository with current submodules. Then you need to create some release config e.g. release_config.yml on you disk. Release config format can be found here. Devices, boards or kits names referenced in release config are case sensitive!

詳細を読む...

件数が多いもの
2 1 2,599
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-982Support adding all folder content recursively

        Generator now supports adding all files and all files of its subfolders under some directory recursively with wildcard.

詳細を読む...

件数が多いもの
1 0 1,667
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v6 are now available.

MCUXpresso Configuration Tools is a product with set of tools that help users of all levels with a Cortex-M-based MCU solution.

詳細を読む...

件数が多いもの
1 0 2,736
nxf46154
NXP Employee
NXP Employee

New versions of MCUXpresso SDK, IDE, and Configuration Tools are now available. In addition to new product support, you will find these updates and enhanced features in the new releases

詳細を読む...

件数が多いもの
0 2 3,809
nxa18344
NXP Employee
NXP Employee

SPDK (Storage Performance Development Kit) is an optimized storage reference architecture. It is initiated and developed by Intel.

SPDK provides a set of tools and libraries for writing high performance, scalable, user-mode storage applications. It achieves high performance by moving all of the necessary drivers into userspace and operating in a polled mode, like DPDK.

詳細を読む...

件数が多いもの
0 0 3,260
lpcxpresso_supp
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso IDE v11.0.0 (build 2516) is now available.

This is a major new version of the IDE, and contains many new features and enhancements over the previous MCUXpresso IDE v10.3.1 and earlier releases. The attached presentation, recommended viewing for all users (new or experienced), provides an overview of many of the major changes, as well as things to be aware of when upgrading from an earlier release

詳細を読む...

件数が多いもの
5 0 6,415
lpcxpresso_supp
NXP Employee
NXP Employee

This article discusses the use of SDK Trustzone example (Hello World) for the LPC55S69 MCU within MCUXpresso IDE.

The following are required to follow this blog post:

  1. MCUXpresso IDE Version 11.0.x
  2. LPCXpresso 55S69 EVK development board
  3. LPCXpresso 55S69 EVK version 2.6 SDK
詳細を読む...

件数が多いもの
0 0 5,247
lpcxpresso_supp
NXP Employee
NXP Employee

When using the QN9080 with SDK v2.2 2019-01-29, or earlier, there is an issue in the SDK internal data which can lead to MCUXpresso IDE v11.0.0 failing to set consistent floating point options when importing multiple examples.

詳細を読む...

件数が多いもの
1 0 1,997
hemantagrawal
NXP Employee
NXP Employee

  • Disable hw_prefetch (u-boot):

setenv hwconfig 'fsl_ddr:bank_intlv=auto;core_prefetch:disable=0xFE'

qixis reset altbank (reset the board - in case using bank 0 run 'qixis reset' only)

 

  • bootargs or othbootargs - add below parameters to bootargs (u-boot).

                  Make sure you see the same in ‘cat /proc/cmdline’ once kernel is booted:

- use 1G hugepages:

default_hugepagesz=1024m hugepagesz=1024m hugepages=6 (or any number)

- isolate cpu's for user space (for the CPUs running DPDK without kernel interference):

isolcpus=1-7

- make sure no rcu stalls and watchdog prints:

nmi_watchdog=0 rcupdate.rcu_cpu_stall_suppress=1

詳細を読む...

件数が多いもの
0 0 3,158
BlackNight
NXP Employee
NXP Employee

With the cost of an single pin, many ARM Cortex-M boards including the NXP i.MX RT1064 can produde SWO data: think about a pin able to stream data out of the chip in realtime.

詳細を読む...

件数が多いもの
3 0 4,222
xiaodong_zhang
NXP Employee
NXP Employee

GmSSL is an open source cryptographic toolbox that supports SM2 / SM3 / SM4 / SM9 and other national secret (national commercial password) algorithm, SM2 digital certificate and SM2 certificate based on SSL / TLS secure communication protocol to support the national security hardware password device , To provide in line with the national standard programming interface and command line tools, can be used to build PKI / CA, secure communication, data encryption and other standards in line with national security applications. For more information, please access GmSSL official website http://gmssl.org/english.html.

詳細を読む...

件数が多いもの
1 0 2,833
nxf47831
NXP Employee
NXP Employee

New features update:

  •  SDKGEN-967Support to automatically hide doc files in Xtensa workspace

         Previously for Xtensa toolchain, developers need to use "hidden: true" in yml to hide documentation files in the                 workspace.
         Now generator can filter files by type attribute to bypass doc type file for Xtensa, which means files with .txt .rtf                 .html .htm .readme .pdf .Doxyfile .xls .css extensions will not be added into the Xtensa workspace.

詳細を読む...

件数が多いもの
1 0 1,794
BlackNight
NXP Employee
NXP Employee

In my previous articles I have used the command line on Linux to build and debug NXP MCUXpresso SDK applications. In this article I'm running code on NXP i.MX RT1064 in RAM or FLASH.

詳細を読む...

件数が多いもの
1 0 4,144