NXP Tech Blog - 第12页

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP Tech Blog - 第12页

BlackNight
NXP Employee
NXP Employee

If you have already Kinetis Design Studio v3.x installed on Linux, then you might run into a P&E driver installation problem while installing MCUXpresso IDE v10.0.0 build 344.

阅读更多内容...

更多
0 0 3,631
BlackNight
NXP Employee
NXP Employee

The following blog post gives a tour through some of the features in the NXP MCUXpresso IDE:

MCUXpresso IDE: Unified Eclipse IDE for NXPs ARM Cortex-M Microcontrollers | MCU on Eclipse 

阅读更多内容...

更多
0 0 1,408
justinbmortimer
NXP Employee
NXP Employee

I am humbled and energized after spending a week with 30,000+ engineers at this year’s Embedded World!

Amazing.  That’s the only way to describe the passion and enormity of our LPC FANS across Europe.  LPC is deep-rooted in the hearts of many and I am lucky to be a part of this inspired, tightknit community.    Embedded World has a strong place in the heart of LPC. 

My personal highlights from the event .... LPC FANS, What's Popular, MCUXpresso & Geoff.

阅读更多内容...

更多
1 2 12.9K
brendonslade
NXP TechSupport
NXP TechSupport

We gave out 200 of our LPC800 DIP breakout board (with an LPC824 installed) at Embedded World last week ... they were snapped up pretty fast! For those lucky folks who grabbed one, here is the schematic. Pretty simple stuff, probably actually easier to read on the packaging!

阅读更多内容...

更多
2 0 57.2K
rocky_song
NXP Employee
NXP Employee

Some days before, there is a great post about LPC dual-core, LPC key feature_DualCore 

This time, we show a LPC5411x based dual-core example. It shows all aspects about dual-core development, startup, communicate, sync, mutex. Enjoy it:)

After extracted the attachement, it locates at "boards\lpcxpresso54114\multicore_examples\blinky\mdk\blinky.uvmpw"

阅读更多内容...

更多
0 5 5,852
justinbmortimer
NXP Employee
NXP Employee

The year when two titans came together forming what is now the #1 supplier to the broad based MCU market.  To the industry, it was the year of the merger, clouded in uncertainty.

阅读更多内容...

更多
0 1 7,405
justinbmortimer
NXP Employee
NXP Employee

Our global ecosystem - from NXP field engineers to distributors and partners are training up on LPC and now more specifically, the newest LPC546xx family.  

But we also want to make sure the engineers actually using our MCUs in their application receive the same information directly from us ... we will continue to keep you updated & informed.

阅读更多内容...

更多
2 1 2,057
brendonslade
NXP TechSupport
NXP TechSupport

ARM just released some new, very thorough tutorials on how to use the LPCXpresso54114 board with MDK. Thanks to Bob Boys for this great work! Check them out at http://www.keil.com/appnotes/docs/apnt_294.asp

阅读更多内容...

更多
1 2 2,021
jessegarcia-b45
NXP Employee
NXP Employee

MCUXpresso IDE is now recommended for all LPC Cortex-M based MCUs. This tool is free to use and does not have any application code size limits. The following blog is provided for informational purposes only.

 

Links to material being referenced:

 

LPCXpresso IDE Download

阅读更多内容...

更多
1 0 2,981
jessegarcia-b45
NXP Employee
NXP Employee

In case you missed it, we extended our low cost LPC800 series, back in September with the addition of the LPC83x family. The LPC83x family introduces new functionality to our streamlined LPC800 series, which includes LPC81x and now LPC83x.  If more functionality is needed, our extremely popular superset LPC82x family is likely the one you need.

The LPC800 series is great 8- and 16-bit alternative for use in various systems, such as end node connectivity, gesture sensing for HMI, basic motor control, power line communication, battery power management … applications are endless from IoT smart home to building control, industrial automation, children’s toys, and more.

 

阅读更多内容...

更多
0 0 1,608
justinbmortimer
NXP Employee
NXP Employee

So I am getting ready for Electronica and brought a bunch of boards home.  I was testing and packing everything when my daughter got her hands on one of the demos ... this is what happened.

阅读更多内容...

更多
0 0 1,444
justinbmortimer
NXP Employee
NXP Employee

Our first software development kit (SDK) based leveraging the nice touch display Smiley Happy  ... it may look simple, but the board is alive and working well! 

阅读更多内容...

更多
2 2 2,396
justinbmortimer
NXP Employee
NXP Employee

If you haven't heard, our LPC54000 power-efficient platform is expanding to address what our 10,000+ customers have been waiting for patiently ... an extension to some of our most popular devices in the market, including LPC1700.

The time has come ... lead customers are developing on the LPCXpresso54608 board now!

阅读更多内容...

更多
2 12 5,335
justinbmortimer
NXP Employee
NXP Employee

Hi!  we love staying connected with all of our LPC customers, which is why it would be great if you could follow our LPC MCU community by clicking on the link from the main forum page.  This allows us to stay better connected and ensure you always receive the latest information direct from the product line.   Portfolio updates, announcements and more will be shared, so stay tuned.  By the way, we have a few design challenges planned and definitely want to make sure you hear the latest details as they are shared.  You can stop following at any time.

 

阅读更多内容...

更多
0 0 1,580
justinbmortimer
NXP Employee
NXP Employee

Whooohooo  ... LPCXpresso54608 boards have arrived! ... development teams are hard at work finishing our release and preparing demos, lead customers have them in hand and we're looking good for our full market launch!  I can't wait for all of you to get a board in the coming months, so you can start developing and sharing what you have using the latest LPC MCU

阅读更多内容...

更多
2 1 1,933
justinbmortimer
NXP Employee
NXP Employee

The newly assembled LPC team has been working hard since day one and now, we are ready to unveil our official plans!

As we approach our relaunch, which starts this November, we will be sharing all of the details on this forum with our 10,000+ customers.  First up, the 2017 product roadmap ... followed by regular updates on LPC5460x, our upcoming launch, which kicks-off our busy year of product announcements and launches.

阅读更多内容...

更多
2 0 1,432
justinbmortimer
NXP Employee
NXP Employee

Dear LPC and Kinetis customers, partners and enthusiasts,

It has been roughly 9 months since LPC and Kinetis merged under the new NXP. Both LPC and Kinetis teams are now under the same business line. Everyone has been working diligently to make sure the basic infrastructures are not broken and customers using either LPC or Kinetis are well supported.

We hope word has gotten out that both product families are doing well.  We have you to thank.

阅读更多内容...

更多
1 0 1,876
brendonslade
NXP TechSupport
NXP TechSupport

For those LPC users who are new to CAN bus, our partners Embedded Systems Academy have scoured the old LPCWare content and newer NXP Community postings to create an extensive set of FAQs. You can use the Community search facility to help find your answers or just browse (select the CAN category to filter down to just this topic). Enjoy!

更多
0 0 1,385
brendonslade
NXP TechSupport
NXP TechSupport

Just released, this new app note is essential reading for power-conscious LPC fans using the flashless version(s) of the LPC1800 series. 

阅读更多内容...

更多
0 0 1,381
brendonslade
NXP TechSupport
NXP TechSupport

Here in the LPC team we are really excited re-energizing the LPC800 family and are working hard to help customers who want to make the transition from 8 and 16-bit MCUs to the Cortex M0/M0+. To this end we've created code bundles which consist of software examples to teach users how to program the peripherals at the basic level.

阅读更多内容...

更多
2 2 4,254
brendonslade
NXP TechSupport
NXP TechSupport

Well folks, the resurgence of LPC continues! I'm pleased to let you know the LPCOpen packages for LPC43xx have been updated, fixing a bunch of issues and improving/correcting the readmes for the examples. In case you didn't know, we have all the LPCOpen packages on the LPC site now; you can find them using the search box, from the part page (under the Software tab) or from the board page. Look out for more LPCOpen package updates over the coming months. The updates are for the currently available LPC43xx boards from NXP (LPCXpresso43xx boards, Keil MCB4357, NGX Xplorer4337 and Hitex LP4350).

阅读更多内容...

更多
1 0 2,271
sruthyuk
Contributor I

Dear friends,

 

I have been trying to test the can_ loop back_ node in KINETIS512_SC_100MHz.zip file by using flexcan1 in TWR-K60F120M module.I have used A47 & A48 primary elevator connections for flexcan1 as shown in freescale user guide. But i dont know how to test the CAN transmission by enabling loop back node

阅读更多内容...

更多
0 0 2,987