We are pleased to announce that MCUXpresso IDE v10.2.0 (build 759) is now available.
This is a major new version of the IDE, and contains many new features and enhancements over the previous v10.0 and v10.1 releases. The attached presentation, recommended viewing for all users (new or experienced), provides an overview of many of the major changes, as well as things to be aware of when upgrading from an earlier release
阅读更多内容...