Hex file settings in MCUxpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hex file settings in MCUxpresso

vishakhadakhane
Contributor III
1 1 10.6K

Hello everyone, I am working on MCUxpresso and using LPC1769 controller. I am done with Led blinking in MCUxpresso. I have used flash magic to flash the hex file in controller using usb to ttl. But I faced a hex file issue while doing this project. So I thought I should share this with everyone who are facing the same issue. After compiling only .axf was getting created. For creating .hex file ,you need to do following settings:

 

1)Go to properties---> C/C++ Build --->Settings ---> Build Steps

 

Now in post build steps :

 

Change

 

arm-none-eabi-size "${BuildArtifactFileName}"

 

# arm-none-eabi-objcopy -v -O binary "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin"

 

# checksum -p ${TargetChip} -d "${BuildArtifactFileBaseName}.bin

 

to

 

arm-none-eabi-size "${BuildArtifactFileName}"

 

# arm-none-eabi-objcopy -v -O hex "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.hex"

 

# checksum -p ${TargetChip} -d "${BuildArtifactFileBaseName}.hex"

 

 

 

2) After  doing step 1, please check if axf is selected in Artifact extension as shown below:

 

pastedImage_1.png

 

 

 

3)For creating hex file go to Debug-->.axf file-->Right Click-->Binary Utilities-->Create hex. Now you are ready to flash! 

 

pastedImage_4.png

 

 

 

Also kindly check this article:MCUXpresso IDE: Creating Binary Files (S-Record, Intel Hex, Binary) 

 

 

 

After doing these settings I got the hex file and finally it worked!!Smiley Happy

标记 (3)
1 评论