when open the file bldc_ref_sol.pmp in MCRSP_BLDC_V1.3.0/freemaster folder,pop up a error information:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when open the file bldc_ref_sol.pmp in MCRSP_BLDC_V1.3.0/freemaster folder,pop up a error information:

1,465 Views
zhijunwu
Contributor I

Using FreeMaster 2.0, when open the file bldc_ref_sol.pmp in MCRSP_BLDC_V1.3.0/freemaster folder,pop up a error information:

   The associated file handle with C:\NXP\MCRSP_BLDC_V1.3.0\freemaster\bldc_ref_sol.pmp is incorrect.

and then close this information, FreeMaster also closed.

what's matter with it? open other .pmp file have not this problem.

the following picture is the real situation:

pastedImage_1.png

0 Kudos
2 Replies

1,181 Views
john_floros
NXP Employee
NXP Employee

What version of Freemaster are you using?  Try downloading the latest installation of Freemaster and install it.  It may fix you issue.  Once you have installed the latest version under help it should have the version 2.0.2.4  listed.

1,181 Views
zhijunwu
Contributor I

Hi,John,

I update the FreeMaster version,and this problem have fixed,thank you for your adivce .

0 Kudos