when I'm compiling an example of MBD, I got this error, Undefined function or variable 'lic_err'.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when I'm compiling an example of MBD, I got this error, Undefined function or variable 'lic_err'.

Jump to solution
1,180 Views
jwsmarte
Contributor II
What should I do to get rid of it? Thanks! 
TIM图片20170916094650.png
Labels (2)
0 Kudos
1 Solution
856 Views
jwsmarte
Contributor II

ok!Problem was solved with the following post.

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the file attached in the following folder 

{Toolbox install dir}\mbdtbx_pnt\mbdtbx_pnt\mscripts\matlab_ui\ folder mbd_pnt_hostid.p file

 

Customer Report: Undefined function or variable 'lic_err'.

View solution in original post

1 Reply
857 Views
jwsmarte
Contributor II

ok!Problem was solved with the following post.

HotFix_2: Fix license errors for DISK_SERIAL_NUM with less than 8 characters

NXP Tracking numberAST-619

 

Problem: If your HDD has a serial number with less than 8 characters, the license checking and validation will fail even if the license is correctly generated

 

Root Cause: Coding logic error

 

Workaround:  Update the file attached in the following folder 

{Toolbox install dir}\mbdtbx_pnt\mbdtbx_pnt\mscripts\matlab_ui\ folder mbd_pnt_hostid.p file

 

Customer Report: Undefined function or variable 'lic_err'.