the eTimer module configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the eTimer module configuration

1,005 Views
hjhjhj
Contributor IV

Hi Daniel,

        I try to configure the eTimer module to read more input pins,such as A4,A5,A6,A7,A8,F0 and D14.But only the input pin A0 is availble.It's possible that there's some problem in my configuration.Can you help me find it?The HW I used is MPC5744P DevKit.

 

Thanks!

Hj

0 Kudos
3 Replies

786 Views
mariuslucianand
NXP Employee
NXP Employee

Hello hjhjhj‌,

Let's try like this: please replace in the {Path where you installed the toolbox}\mbdtbx_pnt\src\c_library the .c attached file (an advice would be to rename the existing one and keep it  in case the one provided is not ok) and then try to test your model or the one attached.
I'm looking for your response to see if this worked or not.

Hope that helps, 

Marius

0 Kudos

786 Views
hjhjhj
Contributor IV

Hello Marius,

      Sorry for delay.The model  attached work,but the pins A0,F0,D14,A4 always work at the same time and the any of pins A5,A6,A7,A8 affects the four pins A0,F0,D14,A4 .Is there any solutions for this.

Thanks!

Hj

0 Kudos

786 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi hjhjhj

We are looking into this. Stay tuned - we will update soon!

Thank you!

Daniel

0 Kudos