bsc9132 network card drive In the Linux kernel

cancel
Showing results for 
Search instead for 
Did you mean: 

bsc9132 network card drive In the Linux kernel

152 Views
zhengguangzhe
Contributor I

There are bsc9132 network card drivers related to TX, RX four-way matching on the Linux kernel how corresponding, how is the corresponding interface configured?

address:psc9132 

0 Kudos
1 Reply

69 Views
constantinrazva
NXP Employee
NXP Employee

Hello zhengguangzhe‌,

Here on the Model-Based Design community we handle questions regarding our toolbox or other MATLAB/Simulink related questions. I think your question is best suited for the Qonverge community, so my advice is to ask it there (as I can not move it myself).

Hope this helps,

Razvan.

0 Kudos