Why is the UART in Coordinator not working properly in JN5169?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is the UART in Coordinator not working properly in JN5169?

434 Views
1979717461
Contributor III

I created the UART in the Coordinator, but it doesn't work. For example, I send 0xFF through the serial port. However, the content received by the serial port assistant is 0x3F. When sending 0, the serial port cannot receive it. But creating the same UART works fine in EndDevice.I do not know why it has to be like this.

Have you ever encountered this situation? thank you very much for your reply.

Tags (2)
0 Kudos
1 Reply

385 Views
constantinrazva
NXP Employee
NXP Employee

Hello 1979717461@qq.com‌,

Unfortunately on this community we only handle issues regarding MATLAB/Simulink and our toolboxes. I would suggest to post this question in the https://community.nxp.com/community/wireless-connectivity .

Hope this helps,

Razvan.

0 Kudos