[Warning] Wrong Configuration for PBRIDGE Clock in the MBD toolbox 3.0.0 - Devkit MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Warning] Wrong Configuration for PBRIDGE Clock in the MBD toolbox 3.0.0 - Devkit MPC5744P

Jump to solution
959 Views
rafael_barbosa
Contributor IV

Hello,

I am using the Devkit MPC5744P and I could check that the Model Based Design Toolbox 3.0.0 for Simulink has a wrong configuration for PBRIDGE clock.

By default, any model using the MBD toolbox presents the PBRIGDE clock frequency running on 100 MHz. I attached a model that verifies the clock configuration and a Freemaster file in order to make easier the visualization.

However the MPC5744P Reference Manual states that the maximum frequency configuration for PBRIGDE clock is 50 MHz, as can be checked below.

pastedImage_1.png

Kind Regards, Rafael Barbosa

mariuslucianandrei

1 Solution
878 Views
constantinrazva
NXP Employee
NXP Employee

Hello rafael.barbosa@chassisbrakes.com,

I have attached here the new PEBRIDGE config.

The path for the file to be replaced is the following:

{TOOLBOX_DIR}\mbdtbx_mpc574x\src\c_library

Kind regards,

Razvan.

View solution in original post

2 Replies
879 Views
constantinrazva
NXP Employee
NXP Employee

Hello rafael.barbosa@chassisbrakes.com,

I have attached here the new PEBRIDGE config.

The path for the file to be replaced is the following:

{TOOLBOX_DIR}\mbdtbx_mpc574x\src\c_library

Kind regards,

Razvan.

878 Views
constantinrazva
NXP Employee
NXP Employee

Hello rafael.barbosa@chassisbrakes.com‌,

I will investigate this issue and provide a fix for the correct value of PEBRIDGE clock.

Thank you for pointing this out!

Kind regards,

Razvan.