Unreadable symbols in UART from MPC5775B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unreadable symbols in UART from MPC5775B

Jump to solution
1,102 Views
sonik82
Contributor III

It is impossible to recognize messages which sent via UART (uart_hello_world_mpc574xP model) from MPC5775B BMS Plus VCU Reference Design board.

hello 4.PNGhello 3.PNG

There is no any problem when same model is used together with DEVKIT MPC5744P.

hello 2.PNGhello.PNG

0 Kudos
1 Solution
1,089 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @sonik82 ,

We have a model in the toolbox for the MPC5777C which is basically the same as the MPC5775B that you are trying on. I see no problems with this one. Can you please give it a try? Also, I've uploaded the model here.

mariuslucianand_0-1616756304318.png

Hope this helps,

Marius

View solution in original post

4 Replies
1,090 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @sonik82 ,

We have a model in the toolbox for the MPC5777C which is basically the same as the MPC5775B that you are trying on. I see no problems with this one. Can you please give it a try? Also, I've uploaded the model here.

mariuslucianand_0-1616756304318.png

Hope this helps,

Marius

1,067 Views
sonik82
Contributor III

@mariuslucianand  Thank you, uart_hello_world_mpc5777C works fine.

0 Kudos
1,079 Views
sonik82
Contributor III

@mariuslucianand  Thank you for information about MPC5777C UART hello world example model. I didn't know about this model because it is not in my library.

sonik82_0-1616761710844.png

But I found it in explorer

sonik82_1-1616761763201.png

So today I am going to try this model and let you know results.

 

0 Kudos
194 Views
siegeljb
Contributor I

I'm having the same problem with the MPC5775B Evaluation board, 

it works if I choose the MPC5775C processor, seems the clock is different, but not clear what else is changed.

0 Kudos