S32K144 PIL timeout error while receiving data from the rtiostream interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 PIL timeout error while receiving data from the rtiostream interface

Jump to solution
2,358 Views
liu_madeon
Contributor III

1.    The timeout of 10 seconds for receiving data from the rtiostream interface has been exceeded the error faced after 100% Programming into the MCU (virtualMass laststat show completed) - during PIL execution using MBDTool box w/ [MATLAB 2019a] in devkit S32k144.

I set up the Target connection with default OpenSDA download and opensda connected LPUART1 RX: PTC6 TX:PTC7

2. I tried setup LPUART to 0 with RX:PTB0 TX:PTB1, but it changed to LPUART1 with PTC6 and PTC7 after I apply and click ok and show the target connection again. 

if I want to use other UART port how could I setup the Target connection?

----------------------------------------------------------------

previous multiple target question is solved by delete slprj generated content and  execute matlab with full administration permission, and this question I already changed add-on directory to root C:/ , thanks your support.

Tags (2)
1 Solution
2,233 Views
liu_madeon
Contributor III

the question already fix by,

install s32k144 mbdtoolbox patch2.

the matlab install directory at C:/  the folder naming without space.

matlab add on   folder name must without  space like matlab-add-on and  locate with the administrator like C:/Users/

View solution in original post

5 Replies
2,108 Views
ykarata1
Contributor IV

Dear @mariuslucianand 

 

Thanks for your quick reply. I changed input and output signals so as to relieve communication line. Since Our dt=0.05 second, communication buffer/line can not catch data speed. So I decreased input/output data and model has worked. Thanks for the suggestion. I will do that as well so as not to run into that kind of issues.

Thanks for your support.

 

0 Kudos
2,234 Views
liu_madeon
Contributor III

the question already fix by,

install s32k144 mbdtoolbox patch2.

the matlab install directory at C:/  the folder naming without space.

matlab add on   folder name must without  space like matlab-add-on and  locate with the administrator like C:/Users/

2,114 Views
ykarata1
Contributor IV

Dear All,

I have MBD installed in "C:\Users\ykarata1\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx"

and Matlab installed in "C:\MATLAB\"

Also I have tried one basic model at PIL and it has worked. But I have tried with one another and it does not works.

But I have got same error. What may be reason for that error? How can I solve that?

 

Thanks.

0 Kudos
2,112 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @ykarata1 ,

I know is strange, but the problem might be the little space from the "MATLAB Add-Ons" since there is the compiler used.

If it is a building error, I've read in your other post that you have moved the MATLAB to a path with no spaces. Can you do this exactly the same with the S32K toolbox files? You can specify to Matlab the AddOns folder location going to Preferences and Add-Ons. May be using a shorter and no space containing path will solve the mentioned issue.

mariuslucianand_1-1611046805856.png

 

If the code builds successfully but you have a timeout problem, then we should investigate somewhere else. Can you be more specific with the problem you are dealing with?

 

Hope this helps,

Marius

 

 

 

2,104 Views
ykarata1
Contributor IV

Dear Marius,

I am trying to work on PIL and the problem that we mention before has attracted my attention.

Now we have 2 single inputs and 2 single outputs. But we need to increase data payload (I was trying to recall that word whole day   ).

Our time step is 0.05 second.

And we need to increase #of data to be transmitted/received. How can we obtain that?

First parameters that I presume that we need to change dt ( I am not sure about that, since PIL does not work real time, I dont believe that will change anything), changing baud rate of serial communication of PIL.

But I believe there should be a way of increasing payload.

 

Any help/support will be highly appreciated.

 

Thanks.Regards.

 

0 Kudos