[S12ZVM32EVB - SCH Ver A2] unable to flash *.sx - file with RAppID bootloader (version 1.6.7.35)

cancel
Showing results for 
Search instead for 
Did you mean: 

[S12ZVM32EVB - SCH Ver A2] unable to flash *.sx - file with RAppID bootloader (version 1.6.7.35)

28 Views
nofake_drstrang
Contributor III

Dear MBD-Team,

after the S12ZVM.rbf is successfully flashed with CodeWarrior/Flash Programmer, I tried to flash application file *.sx with RappID Bootloader Tool, without success. The RappID Bootloader Tool shows  "Init / Erase / Error"

RappIDBootloader_error.PNG

Flash Programmer Console:

.....

Device MC9S12ZVML32_FLASH  
Programming ..........
Device MC9S12ZVML32_FLASH
Program Command Succeeded
Flash Operation. done
cmdwin::fl::device -d "MC9S12ZVML32_EEPROM" -o "512x32x1" -a 0x100000 0x1001ff
cmdwin::fl::image -f "C:\\MatlabAddons\\2020a\\Toolboxes\\NXP_MBDToolbox_S12ZVMx\\tools\\BootLoader\\RBF_Files\\S12ZVM.rbf" -t "Auto Detect" -re on -r 0x100000 0x1001ff -oe off
cmdwin::fl::erase image
-------------------------
Auto-detection is successful.
File is of type Motorola S-Record Format.

Image size is 0 bytes, nothing to erase.
Nothing to erase. No sectors selected
Erase Command Succeeded.
cmdwin::fl::write
-------------------------
Flash Operation. ...
Auto-detection is successful.
File is of type Motorola S-Record Format.

Device MC9S12ZVML32_EEPROM

Programming ....
Programming warning. Can't program 8 bytes to address 0xfffe08 because this range isn't included in the selected modules!
Programming .....
Device MC9S12ZVML32_EEPROM
Program Command Succeeded
Flash Operation. done

I have 2 questions:

1) Is there a How-To / Step-by-Step / Getting Started... documentation for this evaluation board?

2) When to use the Jumper J10 ?

J10

OSBDM boot-loader option
Closing this jumper, the OSBDM enters in boot-loader mode

Thank you!

BR

Alex

0 Kudos
0 Replies