Dear MBD-Team,
after the S12ZVM.rbf is successfully flashed with CodeWarrior/Flash Programmer, I tried to flash application file *.sx with RappID Bootloader Tool, without success. The RappID Bootloader Tool shows "Init / Erase / Error"
Flash Programmer Console:
.....
Device MC9S12ZVML32_FLASH
Programming ..........
Device MC9S12ZVML32_FLASH
Program Command Succeeded
Flash Operation. done
cmdwin::fl::device -d "MC9S12ZVML32_EEPROM" -o "512x32x1" -a 0x100000 0x1001ff
cmdwin::fl::image -f "C:\\MatlabAddons\\2020a\\Toolboxes\\NXP_MBDToolbox_S12ZVMx\\tools\\BootLoader\\RBF_Files\\S12ZVM.rbf" -t "Auto Detect" -re on -r 0x100000 0x1001ff -oe off
cmdwin::fl::erase image
-------------------------
Auto-detection is successful.
File is of type Motorola S-Record Format.
Image size is 0 bytes, nothing to erase.
Nothing to erase. No sectors selected
Erase Command Succeeded.
cmdwin::fl::write
-------------------------
Flash Operation. ...
Auto-detection is successful.
File is of type Motorola S-Record Format.
Device MC9S12ZVML32_EEPROM
Programming ....
Programming warning. Can't program 8 bytes to address 0xfffe08 because this range isn't included in the selected modules!
Programming .....
Device MC9S12ZVML32_EEPROM
Program Command Succeeded
Flash Operation. done
I have 2 questions:
1) Is there a How-To / Step-by-Step / Getting Started... documentation for this evaluation board?
2) When to use the Jumper J10 ?
J10
OSBDM boot-loader option
Closing this jumper, the OSBDM enters in boot-loader mode
Thank you!
BR
Alex