Purpose of "Please restart Evaluation Board" message box?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Purpose of "Please restart Evaluation Board" message box?

Jump to solution
1,837 Views
rsating
Contributor III

Please help us understand the purpose of the message box that says "Please restart Evaluation Board to move processor to BAM mode and press OK", see attached screenshot.  This message box is displayed when we build code in the Matlab/Simulink MBDT examples. 

Is a reset sufficient?  Is it really necessary to power cycle the board?  And why?

Thanks

 

 

Labels (1)
0 Kudos
1 Solution
1,815 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating,

Thank you for your interest in our MBDT Toolbox!

The message that pops up, telling the user to reset the board, asks for a reset from the button, not necessarily power down and power up, in order to set the board in the bootloader. When the MCU boots up, it enters the bootloader (that has to be flashed previously using the S32DS according to the quick start guide). When the processors boot up, it enters bootloader and waits for a five seconds for a new firmware to be delivered over UART. If it receives nothing from the host computer, then the bootloader starts executing the code already stored in the flash memory.

So the mechanism is as follows:

1. Simulink generates and compiles the code, and shows that popup message.

2. The user resets the board and within 5 seconds press the 'OK' button.

3. If everything works fine, the host sends the new firmware to the board and the board boots the new code.

Hope this helps,

Marius

View solution in original post

0 Kudos
2 Replies
1,816 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating,

Thank you for your interest in our MBDT Toolbox!

The message that pops up, telling the user to reset the board, asks for a reset from the button, not necessarily power down and power up, in order to set the board in the bootloader. When the MCU boots up, it enters the bootloader (that has to be flashed previously using the S32DS according to the quick start guide). When the processors boot up, it enters bootloader and waits for a five seconds for a new firmware to be delivered over UART. If it receives nothing from the host computer, then the bootloader starts executing the code already stored in the flash memory.

So the mechanism is as follows:

1. Simulink generates and compiles the code, and shows that popup message.

2. The user resets the board and within 5 seconds press the 'OK' button.

3. If everything works fine, the host sends the new firmware to the board and the board boots the new code.

Hope this helps,

Marius

0 Kudos
1,737 Views
Lavern
Contributor I

Thanks for sharing this answer to us.

Tags (1)
0 Kudos