I am facing problem in code generation. Please check my environment variable path I have directed it to 2 paths.
Hello vikas1.singh@heromotocorp.com,
The GCC_S32K_TOOL environmental variable seems to be the problem.
Can you try and run the following command in the MATLAB terminal:
setenv('GCC_S32K_TOOL', '{INSTALL_ROOT}\tools\gcc-6.3-arm32-eabi')
From what I can see from the log, if I don't have any typos the actual command should be the following:
setenv('GCC_S32K_TOOL', 'C:\Users\mbelec\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\code\tools\gcc-6.3-arm32-eabi')
and try to build again after? If this works, set it in windows (the GCC_S32K_TOOL system env. variable).
Please let us know if you're still having issues with this.
Kind regards,
Razvan.