Does NXP offer DXF file for importing reflow soldering footprint into layout tool (PBSS4130PANP and BCM856BS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP offer DXF file for importing reflow soldering footprint into layout tool (PBSS4130PANP and BCM856BS)

1,247 Views
ChrisDarrow
Contributor III

My customer would like to get the DXF file for easy import into their layout tools. Rather than the customer needing to recreate the layout as NXP has probably already developed the DXF file. Can NXP provide?

When looking at the datasheets for both PBSS4130PANP and BCM856BS, the Reflow Soldering Footprint picture has a reference to the package type (SOT1118_FR and SOT363_FR, respectively). Has NXP already created a DXF or other file that can be imported into my customer's CAD tools rather than them having to create it themselves?

Thanks.

0 Kudos
1 Reply

1,057 Views
raduivan
NXP Employee
NXP Employee

Hello Chris, this community is to support NXP's Model Based Software Design Tools. There is no support here for the products you are inquiring about.

Regards,

Radu

0 Kudos