Hello.community
In my model,ADC1 can be triggered by CTU.
But,It is failed for ADC0.
Can you help solve the problem?
Thank you very much.
best regards
hao
Solved! Go to Solution.
Hello haoxue1027@qq.com,
The model you've sent crushes all the Matlab versions I've tried to run it on. Maybe is because I am using the MBDT 3.2.0 and from the other thread I see that you are using the 3.1.0. Have you considered updating to our latest version?
Why don't you start from our example pwm_ctu_adc_mpc574xP.mdl?
Hope this helps,
Marius
Hello.
Sorry to trouble you,
Can you help me check the problem?
I have further confirmed the model.
The model I have built cannot work about ADC0 and ADC1 even though it is the same configuration as the demo"pwm_ctu_adc_mpc574xP".
But the demo can work normally on the board devkit-MPC5744P.
Is this a bug here?
My matlab version is 2019b.
Thank you very much.
best regards
hao
Hello haoxue1027@qq.com,
The model you've sent crushes all the Matlab versions I've tried to run it on. Maybe is because I am using the MBDT 3.2.0 and from the other thread I see that you are using the 3.1.0. Have you considered updating to our latest version?
Why don't you start from our example pwm_ctu_adc_mpc574xP.mdl?
Hope this helps,
Marius
Hello,Marius.
Thank you for replying.
I will update my version and check it again.
best regards
hao