on the s32v234 eval kit, the voltage of the mipi bus is called out at 1.0V. i see you have camera - sony and ov cameras which use mipi at 1.2V. i think the standard called out 1.2V as well. is it OK for me to use the mipi interface on my sensor at 1.2v and connect it directly to the 1.0v mipi on the eval kit? i think the dc component is removed, but want to confirm this is OK with NXP.
thanks!