What's the difference between S32V234-EVB2 and S32V234-EVB2-D?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's the difference between S32V234-EVB2 and S32V234-EVB2-D?

Jump to solution
1,766 Views
fortunely
Contributor III

I find that there are two S32V234 EVB part numbers from NXP website, that is, S32V234-EVB2 and S32V234-EVB2-D(figure1). But what's the difference between S32V234-EVB2 and S32V234-EVB2-D? 

Does S32V234-EVB2-D own built-in display(LCD)? I don't know whether it neccessory for us to buy an extra LCD screen for  S32V234-EVB2 or S32V234-EVB2-D.I can't find out any documents to ensure the the difference.

Figure1 S32V234EVB Part Number

pastedImage_2.png

Figure2 S32V234EVB Overview

pastedImage_1.png

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,492 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi martinzhang‌,

The main difference is that S32V234-EVB2-D comes with a Plexiglas chassis that has an external LCD mounted in:

pastedImage_1.png 

You can see more it here: Lane Departure ADAS demo on S32V - YouTube 

Anyhow, just recently we have launched the SBC board as well: SBC-S32V234: Vision and Sensor Fusion Platform|NXP 

Hope this helps!

Daniel

View solution in original post

2 Replies
1,493 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi martinzhang‌,

The main difference is that S32V234-EVB2-D comes with a Plexiglas chassis that has an external LCD mounted in:

pastedImage_1.png 

You can see more it here: Lane Departure ADAS demo on S32V - YouTube 

Anyhow, just recently we have launched the SBC board as well: SBC-S32V234: Vision and Sensor Fusion Platform|NXP 

Hope this helps!

Daniel

1,492 Views
fortunely
Contributor III

Hi Daniel,

I get it. Thanks for your help.

0 Kudos