What is the latest version of the Radar SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the latest version of the Radar SDK?

2,637 Views
jane_yu
Contributor I

What is the latest version of the Radar SDK? Is there a newer version than SW32R37-RSDK-RTM-1.1.1?

Thank you!

Tags (1)
0 Kudos
8 Replies

2,223 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi Jane, 

The latest one is  RTM-1.1.1

pastedImage_1.png

Best regards,
Daniel

0 Kudos

2,223 Views
dumitru-daniel_
NXP Employee
NXP Employee

Version 1.2.0 is now available here

pastedImage_1.png

0 Kudos

2,223 Views
jane_yu
Contributor I

Hi Daniel,

Thank you!

I have installed S32R27X-37X_RSDK_RTM_1_2_0, I want to use DCC development kit run 1RF 4Antennas Demo, Which project should I use?

pastedImage_1.png

0 Kudos

2,223 Views
dumitru-daniel_
NXP Employee
NXP Employee

pavelagrigoroaei-b44148‌,

Can you suggest which project is needed ?

Thank you!

Daniel

0 Kudos

2,223 Views
jane_yu
Contributor I

Hi Daniel,

1RF 4Antennas Demo. An error occurs when I built the project,Can you tell me where the problem is?

Thank you!

pastedImage_1.png

pastedImage_3.png

0 Kudos

2,223 Views
b13310
NXP Employee
NXP Employee

Hello, 

could you please clarify for me what method you used to import project - if you had "copy project into workspace" checked?

Best regards

Irina

0 Kudos

2,223 Views
jane_yu
Contributor I

Hi Irina,

I had "copy project into workspace" checked,the method I import project as follows:

pastedImage_1.png

pastedImage_2.png

pastedImage_5.png

pastedImage_4.png

0 Kudos

2,223 Views
b13310
NXP Employee
NXP Employee

Hello,

this is what I suspect.

Could you please try to import it again without this option checked (you would need either remove project you already imported, or use new workspace)

Best regards

Irina 

0 Kudos