Radar FFT processing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Radar FFT processing

1,638 Views
olivierdoare
NXP Employee
NXP Employee

What is the number of points used to perform the range_FFT the doppler_FFT and the reason why you need this number of points

regards,

Olivier

0 Kudos
1 Reply

1,191 Views
iulianbulancea
NXP Employee
NXP Employee

Hi Olivier,

In the example shown Accelerate the Discrete Fourier Transform with NXP SPT  the number of points used for Range FFT is M=512 and for Doppler FFT is N=256, which means that one frame has N=256 chirps, and each chirp has M=512 samples.

In order to perform the FFT algorithm, the number of points (M and N) must be a power of 2. In general, the larger number the better the resolution.

Regards,

Iulian

0 Kudos