RDK-Demo Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RDK-Demo Controller

4,772 Views
burak_
Contributor II

Hi,

I have installed RDK-demo controller on my windows 10 laptop. But when ı try to run program, nothing happens. Program window does not open. In task manager, the task is running. I tried to run it as administrator, nothing has changed. Who can help me solving this issue?

0 Kudos
5 Replies

3,591 Views
Iktler
Contributor I

Are there any new solutions? I had exactly the same problem...

0 Kudos

4,756 Views
longfeiwang
Contributor III

Do you mean it can't be programmed? Or it doesn't run after programming?

0 Kudos

4,752 Views
burak_
Contributor II

I mean, I cannot open the GUI. When ı double click on icon, the application does not open but it is running on background, ı can see in task manager.

0 Kudos

4,750 Views
longfeiwang
Contributor III

You need to install the correct version of the matlab runtime environment and set the correct TFTP directory, then you can run app.exe normally.

0 Kudos

4,721 Views
marmar
Contributor I

I have the same problem. Where should I set the right TFTP directory?

0 Kudos