NXP Vision Toolbox for S32V234 version 1.2.0 - Product Release Announcement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Vision Toolbox for S32V234 version 1.2.0 - Product Release Announcement

NXP Vision Toolbox for S32V234 version 1.2.0 - Product Release Announcement

 

 

 pastedImage_2.png

Product Release Announcement

Automotive Microcontrollers and Processors

NXP Vision Toolbox for S32V234 – 1.2.0

 

 

Austin, Texas, USA

October 14, 2019

pastedImage_1.png

Automotive Microcontrollers and Processors Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Vision Toolbox for S32V234 1.2.0 RFP. This release supports Computer Vision and Machine Learning applications prototyping with MATLAB® for NXP’s S32V234 Automotive Vision Processors.

 

DownloadLocation:

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=NXP_VISION_TOOLBOX

 

Activation link

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=NXP_VISION_TOOLBOX

Technical Support

NXP Vision Toolbox for S32V234 issues are tracked through NXP Model-Based Design Tools Community space

 

 

Release Content (updates relative to previous version)

  • A quick guided tour into the Vision Toolbox main features supported in this release can be watched here:

 Machine Vision Algorithm development using Vision Toolbox | NXP 

  • Compatible with NXP Vision Software Development Kit for S32V2 RTM 1.4.0 libraries and build tools;
  • Machine Learning support with MATLAB® pretrained CNN/Deep Learning Toolbox and code generation for S32V234 ARM A53 now compatible with the latest version of release 2019b;
  • Redesign all ready to run examples that can be executed in MATLAB® simulation or directly on S32V234 HW to make them more user friendly:
pastedImage_5.pngpastedImage_6.pngpastedImage_7.png
  • Faces / Pedestrians / Lanes Detection applications;pastedImage_32.png

 

 

MATLAB® Integration

The NXP Vision Toolbox extends the MATLAB® Computer Vision System, Image Processing and Deep Learning toolboxes experience by allowing customers to evaluate and use NXP’s Vision SDK RTM 1.4.0 and NXP S32V evaluation boards (EVB and SBC) solutions out-of-the-box with:

pastedImage_8.png

 

Target Audience

This release is intended for technology demonstration, evaluation purposes, computer vision and machine learning prototyping with S32V234 microprocessors and S32V SBC & EVB boards

 

Useful Resources

NXP Vision Toolbox Home page

Other useful documents can be found on Toolbox Home page Documentation

 

 

 

Attachments
Comments

pastedImage_1.png

Seems I got an error related with the space in path string when I am trying to exe nxpvt_crate_target command.

Please help.

Thanks,

JD

Hi JimDuan‌,

This is a known limitation of the Vision SDK which does not support spaces in the project directory or SDK directory. You could change the path to one that has no spaces from Home => Preferences => Add-ons:

pastedImage_1.png

Please let me know if you encounter any other problems.

Thank you,

nxf40536

Does this release support camera: MAX9286S32V234 & MCIMXCAMERA1MP (OV10635) yet?

Thx,

Jd

No ratings
Version history
Last update:
‎10-14-2019 09:13 AM
Updated by: