IP address of the board S32V234 Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IP address of the board S32V234 Windows

1,074 Views
willcampo
Contributor III

Hello,
Could someone tell me why I can not find the IP address in this way? .
How else could I find her?

Error_IP.png

Labels (1)
2 Replies

908 Views
paulvlase
NXP Employee
NXP Employee

Hi willcampo@hotmail.com‌,

Did you connect the board to a network?

Do you have a DHCP server on your network that assigns the IP address?  

908 Views
willcampo
Contributor III

Thank you very much for the answer ... Now I have it.
But when it comes to testing the example "face_detection_camera_main", I get the following error.

Error_Face.png

0 Kudos