Datasheet of PTB36241G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Datasheet of PTB36241G

991 Views
chaunm
Contributor I

Hello,

I have a question about the datasheet of PTB36241G

I see the Vth(i) has two value: 75mV (min) and 150mV (max). It mean: The design has only one Vthreshold and it between 75mV and 150mV or the design has two Vtheshold, the signal will be detected when it > 150mV, and won't be detected when it < 75mV?

Thanks,

Chau

Labels (1)
Tags (1)
0 Kudos
1 Reply

899 Views
paulvlase
NXP Employee
NXP Employee

Hi chaunguyen‌,

This community is only for NXP Vision Matlab Toolbox.

We support all technical questions via a ticketing system. Please create a support request for this question at www.nxp.com/support using Support Requests option. This will ensure the correct answer from the subject expert.

0 Kudos