NXP FTF 2016 - トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP FTF 2016 - Training Presentations

ディスカッション

ソート順:
Learn how NXP's Motor Control reference design and control libraries, built on the Kinetis V portfolio, can help you beat pressing design deadlines, improve your time to market, and achieve better motor performance.
記事全体を表示
This presentation describes how to modify an Aarch64 (64-bit) uboot to make it loading an Aarch32 (32-bit) Linux, and how to modify an Aarch64 based Linux to run at Aarch32 mode. The target processor is the QorIQ LS1043A SoC. Watch Video Presentation
記事全体を表示
This technical session provides an overview of the i.MX 6UltraLite MMDC (DDR Controller), the DDR tools used for DDR testing and board bring-up, and hardware considerations for DDR board designs. Attendees should be familiar with the MMDC from previous i.MX 6 series processors, specifically the i.MX 6SoloX. The session covers the differences in the MMDC between the i.MX 6UltraLite and its predecessor, the i.MX 6SoloX applications processor. The first half covers the tool offerings used to assist the user with bringing-up and testing a new DDR interface: i.MX 6UltraLite DRAM Register Programming Aid tool and the DDR Stress Test. The second half of the session covers hardware considerations board designers should follow for DDR board designs.
記事全体を表示
Smart meters are increasingly popular and enhance the supply infrastructure. In this session we will give an overview of smart meter technology, specifically focusing on the sub-GHz RF interfaces. Topics will include typical use cases, overview of system requirements, features of NXP RF Transceiver solutions, and typical (example) customer designs for long range and robustness.
記事全体を表示
Using Accelerometers, Magnetometers, Gyroscopes, gathering Sensor data can be tricky and not straight-forward. In this class, we will go into a Sensor Deep-Dive, where each sensor will be visualized and explained in detail. When collecting data there are several things that can make collecting the data easier, more efficient, and avoiding erroneous data all together. We will have several demonstrations and examples to show the pitfalls and successes of collecting data.
記事全体を表示
Since the early 1920’s, the source of microwave power generation has traditionally been vacuum tubes and magnetrons. Some high power RF applications today still rely on vacuum tube technology, even though there has been a multitude of advances in solid state RF power generation. This class will cover the technological advantages of solid state including dynamic range control, spectral purity, manufacturing economies of scale and product longevity.
記事全体を表示
There are many new technological developments in the medical field that require the use of controlled RF power for several advanced therapeutic treatments. Various levels of RF power at various frequencies are used in procedures such as microwave ablation (tumor destruction), electrosurgery (cut, coagulate, desiccate and fulgurate tissue), diathermy (treatment for rheumatoid arthritis) and thermage (skin rejuvenation). This session will cover innovative RF solutions that NXP has developed for these applications.
記事全体を表示
This technical lecture presents how Toradex built a balancing robot demo application using the new i.MX 7's heterogeneous asymmetric architecture. i.MX 7 features a secondary Cortex-M4, which can be used for real-time or low-power applications. We will discuss how to make use of the secondary core with a FreeRTOS based firmware implementing the closed loop controller to keep the robot balanced upright. On the powerful main CPU complex, a dual Cortex-A7, Linux is running a Qt based user interface. We will go into details about the rpmsg/OpenAMP based messaging offerings provided by NXP. The robot demo application makes use of rpmsg to communicate between the two independently running processor cores and operating systems.
記事全体を表示
Advancing technology has brought down the cost of 24 GHz radar system significantly bringing a whole range of new applications into reach. Historically radar was a pure military and industrial application due to high application costs. With the latest generation of NXP BiCMOS technology this has changed. A 24 GHz radar frontend can now be fully integrated into a single IC bringing the costs and power dissipation down to consumer levels. This opens up a whole range of applications which were previously not possible. This lecture will show the possibilities of radar in different applications such as presence detection and consumer drone collision avoidance. A live demonstration based on first test chips in combination with ARM processors will be given.
記事全体を表示
Gain a deep dive into the GPU and display controller architecture of the i.MX 8 applications processor family. Discover the advanced features, design choices, and the HMI solutions enabled by the i.MX 8 series. This class provides a basic introduction to i.MX 8 graphics and is a precursor to the more advanced i.MX 8 classes around augmented reality, eCockpit, graphics SDK and Vulkan classes. Watch Video Presentation
記事全体を表示
With new CAN FD protocol, CAN applications need to support both classical CAN and CAN FD frames. Especially in transition period, customers are looking for a solution in which classical CAN frames are mixed with CAN FD frames. NXP developed a brand new CAN transceiver feature "CAN FD Shield", which enables the use of CAN controllers in mixed CAN / CAN FD architectures. Watch Video Presentation
記事全体を表示
This is an overview of the next generation S32K microcontrollers family and the system solution benefits using the latest MCU features. Watch Video Presentation
記事全体を表示
This hands-on workshop provides a detailed architecture description of Thread technology and wireless mesh networking. The main Thread concepts will be reviewed and analyzed thoroughly. The attendee will have a deep understanding of the main concepts and how these are mapped to the NXP software API. The session will close with hands-on training to enable the attendee to understand software usage and configuration, low-power features and security concepts.
記事全体を表示
Learn the basics of DDR4 and how to configure the DDR4 controller on QorIQ devices. Watch Video Presentation
記事全体を表示
As consumers embrace the ease-of-use and convenience of contactless payment, global retailers continue to invest in electronic mPOS solutions, with the market projected to grow to more than 80 M installed units by 2018 (IHS Research). mPOS equipment manufacturers need technology designed to address this growth, while meeting security and battery life requirements of the latest mobile payment technologies. The Tower POS development tool (TWR-POS-K81) showcases the capabilities of the Kinetis K81 microcontroller along with the expandable tower system, including the latest NFC controller PN5180 as well as a contact reader interface (TDA8035). A demo application is showing the EMVL1 functionality for NFC and contact transactions. Development tools will be available for all participants of this sessions. Watch Video Presentation
記事全体を表示
Healthcare devices are adopting more and more technology and NXP is at the center of this trend. Learn about the MCUs, MPUs, sensors, and wireless products that are being used in the most innovative healthcare products. Watch Video Presentation
記事全体を表示
The session will provide an overview of the most recent developments to support Radar systems in the frequency range from 76 GHz up to 81 GHz. High level block diagrams and key specifications of NXP multi-channel transceivers will be presented. It will also be discussed how the NXP transceiver solutions can help to enable modern low power consumption sensors with robustness against frequency interference, small size, and high-performance due to scalability. In combination with NXP Radar micro-processors and mircro-controllers typical Radar system architectures will be introduced. Especially for the development of small and compact cocoon, nano radar sensors an example is presented which shows the combinations of NXP Radar tranceivers, NXP Radar processors and NXP power supply solutions. The presentation will also give an outlook to technology trends and future upcoming NXP Radar solutions.
記事全体を表示
Learn how Kinetis V Series MCUs and tools can be used to differentiate your drone applications. PMSM and multi motor control can help suppliers provide longer run times with better control. Combine this performance improvement with the easy-to-use tools now available in the Kinetis V portfolio to provide a single point solution to your drone's speed or gimbal control solution. Watch Video Presentation
記事全体を表示
This session will provide an overview of the QorIQ's hardware root of trust, key protection, and strong partitioning capabilities. Watch Video Presentation
記事全体を表示
The session provides an overview of motion, magnetic field, and pressure sensing applications and the software framework and algorithms needed to mine information from sensor data. In the first hour, the presenter will review common and novel use cases for these sensors. the second hour will provide an overview of technical considerations and common mistakes in collecting and using sensor data.
記事全体を表示