NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
This session will cover emerging trends in crypto acceleration APIs, their benefits, and NXP's roadmap for supporting them. Watch Video Presentation
View full article
This session will provide a demonstration led by the instructor that showcases how you can develop end products using the application solution kit (ASK) for QorIQ LS1043A processors. Watch Video Presentation
View full article
Though cryptographic algorithms like AES are crypto-analytically secure, real implementations must at least be tested against logical attacks such as API misuse. Smart cards and similar devices also face fault and side channel attacks. Such attacks exploit physical effects to manipulate the device or learn about secret information. As these attacks are very critical, customers in the smart card industry ask for third party evaluation (e.g. Common Criteria or EMVCo) to confirm high assurance levels. If passed, a certificate is issued by a trusted party. With the rise of the IoT, physical attacks and respective third-party witnessing of resistance might soon be relevant there as well. Watch Video Presentation
View full article
Healthcare is ripe for disruption. In this class we will outline how NXP IoT products enable a variety of healthcare solutions that will lower patient costs and improve patient outcomes. Watch Video Presentation
View full article
The new USB TYPE-C and PD specification has brought the new possibilities on power implementation through USB port, that will give the end customer a very different experience. At the same time, the new specification has raised the requirements on the power components with higher voltage and higher current. Also the ability to swap current source and change output voltage makes the power structure design even more complex. In order to distribute power in a reliable way on TYPE-C port, NXP has developed a set of Power switches for it. Watch Video Presentation
View full article
CARE enables hospitals and long-time care facilities to better measure, control and manage the overall patient satisfaction by combining a unique NFC-based patient skin-attached sticker and NFC enabled mobile devices with a care application and SMARTRAC's Internet of Things platform SMART COSMOS. The comprehensive solution provides a truly improved patient management, safety and comfort.
View full article
Electronics are part of everything we do nowadays, whether we are talking about mobile gadgets or a space rocket. Regardless of the complexity of the products designed, at some point, they have to be brought to actuality, so they have to be manufactured. This session addresses the impact of some of the most important printed circuit board attributes that affect quality, cost, and lead time.
View full article
Come find out what's next for the QorIQ multicore processor platform. You'll get the latest details on our networking solutions, including and update on the market on our solutions focus.
View full article
This presentation shows case studies of e.g. devices support space savings, low power / low voltage applications and the usage of configurable logics. Associated demo boards will be shown. We would pick some typical examples and show how savings could be squeezed out of them. Watch Video Presentation
View full article
Smart digitalized packaging as a subset of the Internet of Things - a huge trend impacting global packaging industry today. NXP is the Identification industry's #1 chip supplier for smart secure NFC-RFID technology offering a variety of tag ICs from short to long-range, allowing interaction with mobile phones connecting products to the cloud and customers to brands. Watch Video Presentation
View full article
Overview of the QorIQ LS2 and LS1088 processors, including the interfaces supported by the LS family, considerations while designing with these devices and use case examples. Watch Video Presentation
View full article
Learn about NXP's newest technology for Single Chip System Modules (SCM) that provides ultimate customization and tiny form-factor via a unique vertical integration approach. Watch Video Presentation
View full article
The LS1012A is the newest member of the QorIQ LS family, combining high-performance CPUs with line-rate packet processing. Learn more about this new class of product, including the many innovations made possible by its small form-factor and low power dissipation. Watch Video Presentation
View full article
Develop your IoT and wearable applications with Hexiwear, an open source, expandable development platform. The platform is expandable with the option to add 180+ additional sensors through click boards.
View full article
Learn the benefits and advantages of our MAC57D5xx product family, targeted for instrument cluster and industrial human machine interface applications.
View full article
This will be a hands-on session covering the Kinetis Software Development Kit (SDK) and Kinetis Expert using the Kinetis Design Studio Integrated Development Environment (IDE).  
View full article
The standard CAN protocol has been extended into CAN Flexible Data (FD) to provide higher bandwidth while keeping the physical characteristics that have made it the most popular automotive in-vehicle communications protocol . This presentation will provide an overview of the changes to the standard as well as address the challenges faced while rolling out and implementing the technology. Watch Video Presentation
View full article
Lecture on NFC commissioning and various use-cases NFC enables in Smart Home/IoT to save cost and enable convenience. NFC gives best of user experience for installing devices in Smart Home & Buildings and in-addition also useful for Diagnostic, de-commissioning, OTA upgrade and various other useful features.
View full article
Many people involved in the electronics industry need a basic knowledge of semiconductor components in order to understand issues like manufacturing cycle time, semiconductor fab consolidation and failure analysis results. This session is geared towards a non-technical audience and gives a high-level overview of semiconductor devices and how they are made. The lecture begins with a brief overview of how semiconductor devices work. The bulk of the presentation describes the generic manufacturing flow for semiconductor devices with an emphasis on the complexity of the equipment/facilities used and the process time required. Watch Video Presentation
View full article
Get up and running in minutes with the NXP S32K platform using the S32 SDK and S32 Design Studio. This hands-on session will introduce the full flexibility and capability of the S32 SDK package, outlining the excellent out-of-the-box experience, ease of use and shorter time to market. Attendants will learn how to use it in correlation with S32 Design Studio IDE to quickly create suitable applications for general-purpose use-cases, running through all the development steps (installation, software configuration & RTOS integration, inserting application code and target debug).
View full article