SMI-N2027 Toradex- A Balancing Robot Leveraging the Heterogeneous Asymmetric Architecture of i.MX 7 with FreeRTOS and Qt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SMI-N2027 Toradex- A Balancing Robot Leveraging the Heterogeneous Asymmetric Architecture of i.MX 7 with FreeRTOS and Qt

SMI-N2027 Toradex- A Balancing Robot Leveraging the Heterogeneous Asymmetric Architecture of i.MX 7 with FreeRTOS and Qt

This technical lecture presents how Toradex built a balancing robot demo application using the new i.MX 7's heterogeneous asymmetric architecture. i.MX 7 features a secondary Cortex-M4, which can be used for real-time or low-power applications. We will discuss how to make use of the secondary core with a FreeRTOS based firmware implementing the closed loop controller to keep the robot balanced upright. On the powerful main CPU complex, a dual Cortex-A7, Linux is running a Qt based user interface. We will go into details about the rpmsg/OpenAMP based messaging offerings provided by NXP. The robot demo application makes use of rpmsg to communicate between the two independently running processor cores and operating systems.

附件
无评分
版本历史
最后更新:
‎05-25-2016 09:52 AM
更新人: