what's mean of Vgs1 and Vgs2 in the model MHT2012N ?How to simulates it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what's mean of Vgs1 and Vgs2 in the model MHT2012N ?How to simulates it?

1,379 Views
1124481165
Contributor II

pastedImage_1.png

4 Replies

1,275 Views
LPP
NXP Employee
NXP Employee

MHT2012N is a dual stage LDMOS amplifier. It includes integrated quiescent current temperature compensation circuit. VGS1 and VGS2 are reference current inputs for this circuit. VGS1 determines quiescent current of the first stage and VGS2 of the second one.

In NXP reference design, the reference currents are generated using 4.7kOhm resistors as current sources. VG1 and VG2 voltage should be tuned to achieve required quiescent drain currents through VDS1 and VDS2 pins.

Note. MHT2012N model kit for ADS does not emulate temperature compensation circuit. The model's Vgs1 and Vgs2 represent internal gate voltages rather than reference current inputs. In contrast to real device, Vgs1 and Vgs2 pins are high impedance inputs and do not sink current. You should connect these pins to voltage sources and tune these voltages to achieve required drain currents. 

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,275 Views
1124481165
Contributor II

Thanks a lot! But I still don't know how to connect it in ADS? what's the function of VT_stg1 and  VT_stg2?

pastedImage_1.png

0 Kudos
Reply

1,275 Views
LPP
NXP Employee
NXP Employee

Please, I can share a document on this topic.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,275 Views
1124481165
Contributor II

Oh!Thank you very very much!

0 Kudos
Reply