Unable to read the SRAM of NT3H2111 in pass-through mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to read the SRAM of NT3H2111 in pass-through mode

823 Views
last_time
Contributor I

Hi,  everybody:

There is a problem in using NT3H2111.

I use the pass-through mode, and the SRAM_PROT bit is set.

I can write and read the SRAM of NT3H2111 using CLEV6630A in pass-through mode.

I can't read the SRAM when using a phone, but I can write it.When the SRAM_PROT bit is clear, I can read it.

Look forward to your reply. thanks!

Labels (1)
0 Kudos
1 Reply

758 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bruce Lee,

We provide an app note on that topic, please kindly refer to https://www.nxp.com/docs/en/application-note/AN11579.pdf  for details.


Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos