The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

3,246件の閲覧回数
marco_li
Contributor I

The installation of S32 Design Studio for Power Architecture Version V2.1 has been rolled back.

The attached file is the installation log.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,369件の閲覧回数
Hwanmin
Contributor II

Hello.

Could you tell me how to check the access? I'm having the same problem. Thank you.

0 件の賞賛
返信

3,102件の閲覧回数
marco_li
Contributor I

The screenshot is as below:

pastedImage_1.png

0 件の賞賛
返信

3,102件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello marco.li@zongmutech.com‌,

In the installation instructions, it is stated that the user must have administrative access when installing S32 Design Studio for Power Architecture. Without this, there will be access denials during installation which will trigger the rollback. This is seen in the log file provided:

Install Uninstaller: S32 Design Studio for Power Architecture Version 2.1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Could you please confirm if the tool was installed with administrative access enabled?

Best Regards,

Mike

0 件の賞賛
返信