TEA19161 LLC调试出问题了

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA19161 LLC调试出问题了

5,561 Views
cetacean
Contributor I

1、TEA19161调试LLC时,SNSBOOST(#16脚)外加+2.5V电压,SUPIC(#1脚)的电压只有+5.4V,SUPREG(#5脚)的电压只有+4.4V,同时接SUPHV(#8脚)的24K电阻(多个1206的贴片电阻串联,功率足够)上的焊锡融化了。

2、SNSBOOST(#16脚)通过分压电阻接在DC+(整流滤波后的)上,SUPIC(#1脚)的电压也只有+5.4V。

3、电路是按照DEMO的设计(高频变压器比34:3:3:15:15,输出90V3A),保护都禁用了。电路无电压输出。

请帮解决?谢谢!

0 Kudos
Reply
0 Replies