SJA1105 can be used between two mcu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SJA1105 can be used between two mcu?

1,724 次查看
caolejun
Contributor I

Hello,

My Pcb has two MCU:S32V234 and TC297. If I use a SJA1105 to connect this two mcu, is it OK?

0 项奖励
回复
3 回复数

1,649 次查看
Bulat
NXP Employee
NXP Employee

Yes, it is ok.

Regards,

Bulat

0 项奖励
回复

1,649 次查看
caolejun
Contributor I

Thank you Bulat Karymov!

So I chose TC297 to control SJA1105 by SPI,then in my code:

1. Should TC297 initialize SJA1105 first?

2. S32v need initialize SJA1105?

Thanks! 

0 项奖励
回复

1,649 次查看
Bulat
NXP Employee
NXP Employee

The SJA1105 is configured via SPI, so it should be configured by the controller with SPI connection to the switch.

Regards,

Bulat

0 项奖励
回复